We have below some questions on the internal thermal-overload protection of UA78M33IKVURG3. Please help.
1. Is there OTP function on UA78M33IKVURG3?
2. If there were OTP function or similar, what value is the value when over-temperature triggered?
3. What is the exact function mechanism of the “internal thermal-overload protection” as stated in the data sheet? How does the IC work when overload or over temperature happen?
Could the operation be explained how the current or load can be limited when temperature was too high? What is the exact relation or values?