Part Number: LP8860-Q1EVM
Hi,
I am currently setting up in Cluster Mode to control 4 LEDs strings independently. I have set the brightness to all 4 registers to 0xFF since I would like to use the Current registers to control the brightness of the LEDs. I have disabled the EN_DISPLAY_LED_FAULT and have enabled the EN_CL_LED_FAULT. When I program the current registers to a value close to 0x00 I am getting a SHORT_LED fault. The following are the settings of the EEPROM Registers:
Address Value
0x60 0xE0
0x61 0x00
0x62 0xDC
0x63 0x4F
0x64 0xDF
0x65 0xE5
0x66 0xF2
0x67 0x77
0x68 0x77
0x69 0x71
0x6A 0x3F
0x6B 0xB7
0x6C 0x17
0x6D 0xEF
0x6E 0xB0
0x6F 0x87
0x70 0xCE
0x71 0x72
0x72 0xC5
0x73 0xDE
0x74 0x35
0x75 0x6
0x76 0xDC
0x77 0xFF
0x78 0x3E
Is there something I am overlooking that is causing the short?
Thanks,
Sean