hai sir,
i have designed the BMS board as per the EVM refernece design and i am using only 1 board.The board is detected by the GUI but i am voltages of the cells are not visible in gui and the leds corresponding to the balancing circuit is always on as the cels are connected.And as a try t pool file write is showing red and device column , checksum is showing error.I also checked the voltage across test point the voltages are correct I have not changed the register configuration.