Dear all,
I can not do simulation of TPS560200 using WEBENCH.
※condition
Vin=4.5〜5.5V
Vout=3.3V
Iout=0.5A
For classic type of WEBENCH, It was displayed that simulation is not possible due to the following message.
When I check the data sheet, I think that it is possible to operate under the conditions listed above from the following data.
Could you tell me why simulation is not possible?
Best Regards,
Y.Ottey