UCC28780 is Active clamp Flyback ( ACF )controller. But ..... this is the story , for a ~300W ,universal AC input , 300Vdc output isolated conversion application.
discussion among colleague( PM and engr ) for the full load efficiency ; says PFC required , why not use a single stage active clamp flyback for both PFC and power conversion ,
single stage conversion should have better efficiency than two stages ( ex: boost PFC+ LLC , or boost PFC + ACF ) . ( not " apple to apple" , maybe )
But I'm thinking that flyback is naturally single ended that have large core loss , and higher Vds than Vin; plus ACF's ZVS may only effective at certain load range, not to mention ACF behavior will deviate
a lot at extremely wide AC line voltage range for PFC function , supposed can't get ZVS at most of line voltage range; hence, full load efficiency will still much less than two stages like boost PFC+LLC
( eff: 96%x96%= 92%), or boost PFC+ACF ( 96%x 92%=88% maybe? ) . To me, for hundreds wattage off-line conversion, If one stage ACF PFC eff. is good, why there are a lot of two stages solution,
but this is the logic , some people prefer to have more technical reason. my technical thought above may not enough? any good comment from you ? thanks a lot of any advice to me!