Other Parts Discussed in Thread: GPCCHEM
Hello,
We did a test with the GPCCHEM tool. The result is the following:
Chemistry ID selection tool, rev=2.48
[…]
Best chemical ID : 1323 Best chemical ID max. deviation, % : 1.32
Summary of all IDs with max. DOD deviation below 3%
Chem ID max DOD error, % Max R deviation, ratio
1323 1.32 0.5
1325 1.33 0.52
...
Full results : Gauging Parameter Calculator report for input file_ '70232N_zip'.msg
The correspondence is correct, but how do you rate the accuracy of 1.32%?
Do you have a threshold not to be exceeded?
Best regards