This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: CEDV learning cycle current rates

Part Number: BQ78350-R1
Other Parts Discussed in Thread: GPCCEDV

Hello guys,

the project is to obtain the optimal parameters for our battery profile with the CEDV method.

The requirements are:

- 7 amps (lowrate) @ 2.5°C, roomtemperature and 45°C

- 15 amps(highrate) @ 2.5°C, roomtemperature and 45°C

Battery Specs: 

- 4 cells in series 

-14 cells parallel

- 58 volts end of charge 

- 39 volts end of discharge

Now the Problem: If i test the batterypack with 15 amps the BMS switches the battery off, because the cells exceed 60 °C cell temperature. Is it a requirement to make a constant discharge with 15 amps at every temperature or can we vary the current for different temperatures. 

  • Hi,

    The GPCCEDV tool really should use the same current load at each temperature to calculate the optimal CEDV gauging parameters. If 15 amps will shut down the BMS due to a temperature fault, it seems like you need to use a lower value for the high load.

    Best regards,

    Matt