This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120A: GPO configure settings of UCD90120A

Part Number: UCD90120A

Hi TI,
I have a question about . It's a unexpected behavior since I added a input path of logic gate.
The behavier of GPI will be changed to continuous pulse. This is not a correct  behavior we expected.
I'm so confused about why configure settings cause this abnormal behavior. I think GPI is just  a input signal, why UCD90120A's configure settings can change the spurce's behavior ?
GPI12 is a active high signal for thermal alert from systm. Our purpose is UCD90120A to  turn-off  2.5V power rail if thermal alert is triggered.
Could you help to check which incorect settings cause this behavior ? I also attach related waveform and settings for comparing.

Thanks.
Blake

See the attached file of UCD90120A_Settings.pptx

1072.UCD90120A_Settings.pptx