Hello experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello experts,
Hello Akashi,
I think it is best to use the temperature derating vs output current curves. There are many curves in the datasheet and this is real data.
These curves specify the output current for the application condition (ambient temperature, input voltage, output voltage).
Let us know if this makes sense to the customer.
Cheers,
Denislav
Hello Denislav,
Hello Akashi-san,
I strongly believe that the curves in the datasheet are more meaningful than Theta JA spec.
There are many components on the board. Looking at Theta numbers assumes the hottest component is the IC. I don't know if this is the case or not.
Usually the derating curves will take into account all of the components on the module so it is actually more meaningful and more useful.
I will still request from the team if we have specific IC ThetaJA numbers. I hope to have a reply for you early next week.
Cheers,
Denislav
Hi Ryo,
By referencing to the data shown in the figures, a safe operation θjA = 35°C/W
Regards,
Alejandro
Hello Denislav,
Hello Alejandro,
Hi Ryo,
We determine SOA by the following:
(For future reference, the measurement conditions are indicated in footnotes below the figures. I've attached image below)
Hello expert,