This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS82130: Question about typ and min values of EN pin

Part Number: TPS82130


Hi

Is the VIH value of ENpin described in the TPS82130 data sheet correct?
typ : 0.65V, min: 0.9V(Is typ value and min value opposite?)
Is it possible to control the EN pin with 1V?
  • While EN may be read as high for typical values of 0.65V, the minimum value of 0.9V is the guaranteed level above which EN pin will read as logic high. That means that 1V is sufficient to drive the EN pin robustly.