Other Parts Discussed in Thread: TIDA-01638
Dear All,
I designed a power MUX stage using a TPS2121 and I' m facing sime problem.
Here below you can find the TPS2121 portion of the schematic
EXT_PWR is a 6V power source while USB_PWR is a 5V from a USB port. Priority is given to EXT_PWR ,SYS_PWR switch to USB_PWR when EXT_PWR is lower than 4.75V and return to EXT_PWR if this is higher than 5.25V. Here below you can see what happens when USB_PWR is stable but EXT_PWR is not stable.
If the time interval where EXT_PWR is long enough everything is fine and SYS_PWR switches correctly to USB PWR
Green: EXT_PWR
Red : SYS_PWR
Yellow : PR1
Blue : ST
But if EXT_PWR drops at the same time of the rising edge of ST SYS_PWR do not switch to USB_PWR, it drops to zero Volts and then restart with soft start
If EXT_PWR drops before the rising edge of ST SYS_PWR remain at USB_PWR without any drop.
Can you please suggest a trick to avoid the drop to 0V in SYS_PWR ?
Thanks in advance
Cesare Conte