This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 59
Part Number: TPS54332
Hi Team,The datasheet shows current limit threshold is 6.5A (typical).Do you have response time that inductor current intersects current limit thresold to switch off internal high side FET?Best Regards,Yaita
Yaita-san,
The TPS54332 current limit is cycle by cycle current limit. The current is monitored in real time during the high side FET on time and is detected instantly with only some gate delays. The only exception is if current limit is reached during the blanking time (minimum controllable on time). In that case, the current limit is actuated at the end of the blanking time.
Best Regards,
John Tucker
BSR-MV DC/DC Applications
“Working on an automotive power design? Read the E2E technical article Meet European Commission ADAS requirements with TI DC/DC for device recommendations and other helpful resources.”