Hi Experts,
Where can I get documentary of 2p interleaved forward on ti web site?
Other question ,I noticed that there is not offer other device options with this code, if I used UCD3138064 how to select device for UCD3138064 ,thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
Where can I get documentary of 2p interleaved forward on ti web site?
Other question ,I noticed that there is not offer other device options with this code, if I used UCD3138064 how to select device for UCD3138064 ,thanks.
Attached are the schematic and the User Guide/Test report. I will look at code for UCD3138064 and let you know.
Regards,
You can configure the type of device you compile the code for through the file overall_configuration.h
It seems like the code is set for UCD3138064 as default. But you can change by modification of the following part:
#define UCD3138 0
#define UCD3138A 0
#define UCD3138064 1
#define UCD3138064A 0
#define UCD3138A64 0
#define UCD3138A64A 0
#define UCD3138128 0
#define UCD3138128A 0
Regards,
Hi Yitzhak,
Thanks for your replies,but I didn't find overall_configuration.h file with this code, do we look the same code?
please have a look at attached fw,thanks.
I guess these are not the exact same code projects.
The changes for 064 are not big.
Mainly the header and linker files should be replaced and some minor changes in the source code.
Let me see what can I do for you. It may take some time.
Regards,
Hello,
I do apologize for the delay caused.
Just writing to you to let you know that I have not forgot to send you the code.
As mentioned before you can as well modify the code that I have already forwarded to you to make it suitable for 064.
We can remotely support you with the modifications required.
If you prefer to wait, then I will most probably send you the code next week.
Regards,
Hi Han,
We are getting the firmware package ready and will send it to you by Tuesday Nov 12th.
Sorry for the delay caused.
Regards,
Hi Han,
Here is the code that you are waiting for.
ITTF-003-windows-installer.zip
Sorry for the delay caused.
Please let me know if any clarifications required.
Best regards,