Part Number: BQ24192I
1. Why there is still switching waveform even if the chip is disabled by pulling /CE pin high?
2. If switching inductor = 1uH, and output capacitor = 10uF, the input current will be around 30mA when the battery is absent.
if the values are chosen as BQ24192i EVM design(2.2uH and 2*10uF), the input current will be about 2~3mA without battery.
Why is that?
Thanks very much for your explanation.