Other Parts Discussed in Thread: UCC29002
Hi guys,
Does this Load Share Controller also work with constant current power supplies? If not is there an alternative that you can recommend?
If there are no Load Share Controllers for CC, are there any that work at 50V?
The goal of this is to be able to balance the load of several lamps onto the different phases of a 3 phase power system.
Ideal scenario for the customer would be as follows:
3-Phase-Power -> Phase Selector -> PFC ACDC -> DCDC -> Lamp
Several lamps with DCDC power supply included in each lamp are distributed and depending on how many are in operation, phases need to be selected to put the load onto. Alternative suggestion are appreciated as well.
Thanks,
Franz