Hi,
I've done some digging through the forums and referenced the sample code, datasheet and appnote. I am running into a problem where the driver is being correctly programming (I checked the FC1 and FC2 using a read) and producing the expected SOUT when latching in data for the memory, but as soon as I send my VSYNC, pause and start the GCLK (knocked it down to 1MHz), the test LED I have connected does not turn on. I am programming the memory with 0xffff ffff ffff as a test and connecting the OUTR0 to a red test led. I am using the correct orientation as referenced in the designs.
Can someone suggest some other debugging techniques, or help me debug this? I would prefer to use this chip instead of build my own led driver.
Thanks,
Lys