Other Parts Discussed in Thread: LM5060
Hello TI experts,
We’re reviewing the OVP calculations of LM5060-Q1 and have some questions as below. Could you please help check and reply to us?
Thank you.
- The R3 resistor calculation formula might have problem in the datasheet, it seems comes a negative value by calculation. Could you please help take a look?
<<Pict in reply pdf file>>
- Can we use the below formula VINmax in datasheet for calculating the OVP limit? Also can we exclude the UVLObias parameter in the calculation?
<<Pict in reply pdf file>>
- There is a hysteresis of 240mV for OVP, how does the OVP work with this hysteresis?
- The behavior, for example a 17V OVP setting, when the input over 17V, the OVP is active to turn off output, and while the input voltage fall down below 16.76V(17V-240mV), then the output will come back, right?
- Have you ever met or had any lesson learn that the practical OVP active point below the OVP calculation point?
- What’s the difference between OVPbias and UVLObias? From the datasheet block diagram, I do not find where is OVPbias current, what’s it’s function and effect?
- When we design OVP, shall we consider both of them or only UVLObias current as spec formula is enough?
- In the TI calculation tool, it only considers UVLObias without OVPbias. Why OVPbias is not considered?
(TI LM5060 datasheet)
<<Pict in reply pdf file>>
(TI design calculator kit)
<<Pict in reply pdf file>>