This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM136-2.5-N: LM136AH-2.5

Part Number: LM136-2.5-N

Hello,

I'd like to know input voltage range of LM136-2.5N.

Is it only necessary to satisfy the operating current(400uA to 10mA) using a serial resistor regardless of the input voltage range? Or should I consider the input voltage range?

If I do not need to consider the input voltage range, can I use it as follows?

Best Regards,

San Choi