Hello,
LMR14006Y min on time is 95ns. swtiching frequency is 2415kHz is tougher condition I think. 2415kHz period is 414ns.
Duty will be around 24% = 95ns/414ns.
When Vout is 12V desired, around 50V = 12/0.24 is max possible voltage I think.
This is no margin. It should be lower Vin will be needed.
When Vin is 36V, I think there is margin and will work. Does my understand correctly?
I tried this in power designer but max input voltage is 25.5V even though I set VIN = 36Vmax.
Please let me confirm if LMR14006Y can support Vin = 36V, Vout = 12V condition.
Best regards,
Toshihiro Watanabe