Other Parts Discussed in Thread: UCC28704, UCC28910
Hi Experts!
I designed a Flyback using UCC28881,
Input power is 300mW,
input DC-rail is regulated at 300V
and I am using a hysteresis control scheme (manipulating the FB pin) to regulate the output voltage at 700V.
However, the efficiency is very low (in the range of 40 ~50%). I know that this IC powers-up from the high-voltage sinking somewhere around 100uA in HVIN pin.
I am trying to limit the peak current to reduce losses and increase the efficiency a bit. Is there any way to do this in this package?
Any other ways to increase the efficiency?
Thanks!