This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 0
Views: 254
Hello,
We are in the process of adding the FIT rates for our isolated gate drivers to our on-line tool, available at: https://www.ti.com/quality/docs/estimator.tsp
In the meanwhile, below are the FIT rates for our isolated gate drivers from TI.
The following failure rates are summarized by technology and mapped to the associated material part numbers. The failure rates are highly dependent on the number of units tested, therefore, it is not recommended to compare failure rates.
Device
FIT
UCC21750-Q1
0.4
UCC23313
UCC21540A
0.6
UCC21732-Q1
UCC23511
UCC5390-Q1
UCC20225A-Q1
UCC20225-Q1
UCC21530
UCC21530-Q1
UCC21750
UCC21710-Q1
UCC21540
UCC21541
UCC21220A
UCC23513
UCC21222
UCC21222-Q1
UCC21220
UCC21520-Q1
UCC5350
UCC5390
UCC5310
UCC5320
UCC20225
UCC21225A
ISO5852S-EP
0.5
UCC20520
UCC21521
ISO5451-Q1
ISO5452-Q1
ISO5851-Q1
ISO5852S-Q1
UCC21520
ISO5452
ISO5852S
ISO5451
ISO5851
If you have further questions, please start a new thread and we will assist you.
Best regards,
Don Dapkus
Gate Driver Applications
Dallas, TX USA
We have an excellent training series that can help answer all your questions about our gate drivers. It is indexed so you can jump right to the section you want! You can find it here. A second series focused 100% on Isolated Gate drivers may be found here.
We also provide models for our gate drivers to accelerate your time to market. You can find them in the Product Folders under the "Design and development" tab: