Other Parts Discussed in Thread: LP87702
when LP87702 input is 5V,the two bucks have no output,why?
LP87702:VANA=VIN1=VIN2=EN1=NRST=5V。
but VANA=VIN1=VIN2=EN1=NRST=4.2V,the two bucks can work。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
when LP87702 input is 5V,the two bucks have no output,why?
LP87702:VANA=VIN1=VIN2=EN1=NRST=5V。
but VANA=VIN1=VIN2=EN1=NRST=4.2V,the two bucks can work。
Hi,
LP87702 is OTP configurable 2 x BUCK and BOOST device. I assume that we are talking about LP87702DRHBRQ1 device?
This OTP is for 3V3 VIN. When 4.3V VANA, then device Over Voltage Protection happen.
If 5V VIN is needed, it will need custom OTP. Please contact to your local sales team to see if it is possible, thanks
Tuomo
Hi,
our device is LP87702DRHBRQ1.
Now 5V VIN is needed, we try to program the regisster pg_good_level2, the VANA_THRESHOLD bit is set 1, but the device can not work, the outputs of the two bucks is 0V.
Can we modify the registers to acheve the 5v VIN work mode?
thanks
Hi,
Unfortunatelly it can't be changed by user. For the 5V VIN it will need separate custom OTP.
VANA_THRESHOLD is not raise overvoltage limit and that is where you hit if VANA=4.3V or higher
Tuomo