This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150-Q1: FBP pin=1.518V which is higher than the normal value 1.214V

Part Number: TPS65150-Q1

Dear team,

When testing the device, the customer found that the voltage of FBP is 1.518V, but in our datasheet this value should be 1.214V. In addition, the voltage at the DRVP pin is 0V. And the VGH(positive charge pump output) is 27V while the setting value should be 22V. The schematic is as below, Vs=11.6V

When change the diode in the red box to BAV99(larger voltage drop and smaller leakage current compared to the old diode), then the VGH becomes normal. At this time the voltage of DRVP is 0.8V.

Could you please help analyze this problem?

Thanks & Best Regards,

Sherry