Other Parts Discussed in Thread: PMP11090, , UCC28700, PMP10937, UCC28722
Dear Team,
I am looking for a non-isolated HV buck for following specs:
- Input range 297Vdc - 402Vdc,
- 10W / 12V output
- Simple, low BOM count, and preferable non-isolated
For this I came across the PMP11090 (105 to 440VAC Input, 24V/400mA), and was wondering if we can modify the design:
- Removing the bridge rectifier and simplifying the input filter
- changing the 24V/400mA to 12V/0.8...1A
Since it is a controller, I think we could adapt the part of the passives to handle the higher currents in the output part. However, I am not sure if the even higher ratio of Vin-Vout could give some problems?
Any comments are very much appreciated. If you have other options / controllers that are more suitable, I am open to look into the options.
Best Regards
Martin