Dear colleague,
Our custoemr is using PTH12030WAH, but when it has no load current, PTH12030WAH heats up seriously, can't use hand touch.
Schematic as below:
Could you please help us check it?
Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear colleague,
Our custoemr is using PTH12030WAH, but when it has no load current, PTH12030WAH heats up seriously, can't use hand touch.
Schematic as below:
Could you please help us check it?
Thanks a lot!
Hi Rock,
The PTH12030WAH at no load is about 35°C above room temperature; that is normal behavior for this device.
This is due to all of the losses across the device. Majority in regards to the: Switching losses to remain in regulation, core of inductor, and the current circulating.
Keep in mind, this is a dual-phase topology, therefore, all losses are double.
(I reviewed the schematic. It looks okay)
Regards,
Alejandro