Other Parts Discussed in Thread: LM5170
Hi,
I ordered the EvKit a few weeks back and just got to hooking it up. After setting up the jumpers for my mode (buck only, using the onboard voltage loop) and applying 48v, nothing happened. It appears the UVLO line is being held low by shorted pins on the onboard supply regulators U3, U4, and U5. After lifting the EN pin on the LDOs, I can get the UVLO net up to 3.3v using an external supply (but of course the internal 10v supply is off). It seems U5 also has a short in the UVLO pin (but not the enable pin), when the pin is soldered in place I can measure 3.3v across R53.
I'd really rather have the onboard 10v supply for my bench testing, so I'd like to confirm that those 3 parts are the issue and get replacements if possible... though I'm not sure if I'll be able to replace U5 with its thermal pad on the massive power planes and no thermal relief.