Hi,
customer use LMR62421, the shematic as below, and found that the voltage will dorp from 12V to 9.5V when the current change from about 0mA to 800mA(peak).
input: 5V; output 12V, current 800mA(peak)
the waveform as below: yellow is 12V output; green is current.
you can see that when the current start up, the output voltage will drop, the maximum drop to 9.5V.
could you give some suggestions to improve the dynamic response ?thank you