The reference design (EVM board PWR193) uses 22 uF ceramic capacitors C4, C15-C18. Since they are biased at 5 V, the actual capacitance is likely half of the rated one. In addition the ceramic capacitors have piezo effect and can produce high pitched sound.
Is there any reason tantalum capacitors should not be used? I have substitutes tantalum 22 uF 10 V caps on one board and they appear to work just as well.
Thanks.