This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4501-SP: Looking for a QML Space- rated Vreg Vin 10V, Vout 5V

Part Number: TPS7A4501-SP
Other Parts Discussed in Thread: LM2940QML-SP, LM4050QML-SP

My customer is looking for a QML space-rated voltage regulator that can survive 50Krad, has SET and SEE testing, an input voltage of 10V minimum, and an output of 5V (can be variable)? Bonus points for ESD and reverse polarity protection. Something with a lead time that’s not terrible would also be appreciated.

I’ve looked at the TPS7A4501-SP &  LM2940QML-SP, and like both but don’t see any SET or SEE testing

The LM4050QML-SP has SET immunity, but the 60uF cap seems large to me for our application. And it doesn’t have the ESD & reverse polarity protection the other 2 above have.