Hello to everyone,
Is there an indication of min / max undervoltage lockout voltage from the TPS70933?
Thanks and best regards,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello to everyone,
Is there an indication of min / max undervoltage lockout voltage from the TPS70933?
Thanks and best regards,
Brian
Hi Brian,
Unfortunately, the TPS709 does not have a well defined UVLO. We do guarantee that it will operate with VIN down to 2.7V. If VIN is below 3.3V, the device will do its best to regulate VOUT, but the output voltage will be VIN-ILOAD*RDSON (VDO or Drop-out is a function of load current time the effective RDSON of the FET).
I hope this answers your question.
Thanks John for quick response!
Yes, this answers the question.
Best regards,
Brian