Hi team,
I received a question about charge current setting and charge voltage setting.
1. If customer would like to set the charge current to 1024mA, they need to set the resister to 0010000.
After that, if customer would like to add 128mA to the 1024mA to get 1152mA, do they need to set the resister to 0010010(1024mA+128mA)?
Or do they need to just set 0000010(128mA) and it is added to previous 1024mA ?
2. Same question as #1.
When customer originally set the charge voltage to 8192mV(01000000000), after that, if they wants to add 32mV to the 8192mV, do they need to set 01000000010? Or they need just set 32mV(00000000010) and it is added previous 8192mV?
Regards,
Yamaguchi