Other Parts Discussed in Thread: TIDA-00792
Hello to Ti support team ,
I have question according to problems with schematics based on TIDA-00792 . ( I use long time this schematic without problems first time I have problem like that )
I have some amount of new batteries 13S1P that operates different --> After short circuit (~80A) bq7694001 doesn't disconnects FETS , bq7694001 enters to shut down mode due to absence of power and after ~12msec Fets disconnects (due to shut down state) . IC on shut down no 2.5V Power and no communication and only charge wake up the IC . IC proper operates Fets off ~400usec if Load current is lower ~50A and less and IC continue operating .
B.R
Alex.B