Hello E2E,
What is Vout accuracy while loading below 50mA?
or
TPS74901 require minimum load is 50mA for stability?
BR,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason,
Because the TPS749 has a very large pass FET to support the 3A of load current, at very light loads we have a circuit to weakly pull-down VOUT to prevent leakage from VIN to VOUT from raising VIN above its target regulation voltage. My recollection is that the threshold for this mode change is in the 10-20mA range. If you sweep the load current slowly, you would see a small step change in the output voltage. This is the reason we specify accuracy starting from 50mA.
There is no minimum load current requirement as stated in the recommended operating table:
I hope this answers your question.