Other Parts Discussed in Thread: TL431
Hello, I am using the LM431BIM3 in the control loop of a flyback converter. However instead of having a Vref of 2.5V, i am measuring 2.6V instead which makes my output regulates at 12.6V instead of 12V.
R2=4.7k, R1=18k, R3=2.2k, R4=1k, Cz=22n.
The voltage across R3=7V
The voltage across R4=1.1V
voltage across VAK of LM431=3.9V
Can someone help me understand why Vref=2.6V? and how to make it 2.5V? I guess Vref is current dependent..
Thanks