This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180EVM-S05: Why no ground pour or traces under transformer?

Part Number: LM5180EVM-S05
Other Parts Discussed in Thread: LM5180-Q1, LM5180

Hi, I'm laying out a virtual copy of the EVM board and wanted to ask why there is no top copper under the transformer? I assume it is to reduce noise coupling into the ground or traces, but there is still a ground on the bottom of the board which is only 1.6mm away, which would pretty much negate any gains made by removing the top copper???

Also the EVM has a 1nF cap bridgeing the primary and secondary grounds. No mention of it in the data sheet. ??

Also BOM says C8 and C10 are 220pF, but schematic shows 22pF. ??