Other Parts Discussed in Thread: TPS3890
Hi,team
I am looking for an IC to monitor a 24V power supply.
I have two questions.
Q1.
I'm considering TPS3840, but I'd like to ask a question about Equation (8) in the datasheet
Vrail_max = 10 × (10,000 ÷ (10,500 + 10,000)) = 20.5V
Equation 8 is written as above, but isn't “10 ×” correct instead of “10 ÷”?
Q2.
If there is another IC suitable for 24V power supply monitoring, please introduce it.
It is necessary to have OD output and CT terminal.
It is more desirable to use an IC that can adjust the monitoring voltage by dividing the resistance.
thanks.