This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3801: Thermal Resistance

Part Number: TPS3801

Hi,

Is there any information regarding the thermal resistance of TPS3801-01? It is not addressed in the data sheet. If there is more general information about the more general thermal performance of the SOT-70 package that would be helpful too.

Regards,

Garret

  • Hey Garret,

    We have not gotten around to adding thermal data to this datasheet yet, but I can provide you with thermal data here for the DCK package:

    Thermal Data for TPS3801DCK
    RθJA 260.5 °C/W
    RθJC(top) 96.9 °C/W
    RθJB 47.2 °C/W

    ψJT

    2.9 °C/W
    ψJB 46.4 °C/W
    RθJC(bot) n/a °C/W

    Thanks,
    Abhinav.