Other Parts Discussed in Thread: TPS61023
Now we testing tlv61048 and have some problem.
test condition : use Li-ion Battery(3.7~4.2V), output=5.2Volt, 600mA
1. Output Enable : Even if the enable signsl is set low, the output remains constant from 5.2V to 3.2V.
I wnat to zero volt ( Power Consumption zero )
2. Output current : Operate at 5.2V/100mA and operate 600mA, voltage drop to 3.2V.
3. Output voltage : When the powwer switch is on, the output to 3.2V. When the peripheral circuit operates,
it goes up to 5.2V. ( unstable operation )