Hello!
I use a portable sound amplifier in the device.
The device is powered by a 0.9 - 1.3 V battery
I use a op amp with 2.8V , for this I need a boost converter.
A TPS610993 with 3.0V output voltage converter was selected.
But the noise of the converter appeared in the audio path.
The load current for the output voltage of the converter is not more than 0.5 mA.
I tried using the LDO on 2.8V and it helped a little, the noise became smaller, but they did not disappear, and this is especially noticeable when I remove the input signal and start hearing the high-frequency noise of the converter.
When I looked at the oscilloscope, the output voltage after the LDO became more stable, but the input voltage became noisy.
How can I solve this problem?
Thanks!