This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3702: Rpu value and question about IUV(min)

Part Number: TPS3702
Other Parts Discussed in Thread: TPS3700

Hi Team

   As you can see in the picture, I used 10K as the value of Rpu in my design. But in the datasheet of TPS3702, the range of IUV is 0.3mA to 10mA. so I want to ask;

1. If I used 10K as the value of Rpu in my design, the IUV is 0.33 which is closed to the IUV(min), is there any risk when IUV closed to the IUV(min)? please kindly explain it specifically.

2. Why you put the IUV IOV current limit in the datasheet, it seems that this spec won't cause any issue when use the TPS3702, could you help me understand that?

Thanks

Best reagrds

Wesley huang

Wesley-huang@ti.com