Other Parts Discussed in Thread: LMR36506
Hi there
We use LM46002 to convert Vin=19V~12.6V to Vout=11.7V/1A, use ext. freq. 800khz (also connect RT=53.6Kohm at the same time).
When vin=12.6V/no-load, the SW node waveform indicated that converter works in decreased switching freq. ~401KHZ, and it further decreased to 258KHZ when load is 1A. Everything else (like Vout ripple and loop stability) seems remain ok.
We checkd with datasheet to confirm this "frequency-decreasing" behavior when Vin is near Vout. Section 8.3.8 may give the explanation that under 800KHZ freq, we will hit the Dmax = 84% limit. So we can not get 11.7V from 12.6Vin with 800KHZ because of "frequency foldback". It seems to be reasonable behavior of LM46002.
Could you please tell how this "frequency foldback" works? We have to ensure f_switching=800KHZ for all DC/DC in our system, and "12.6V to 11.7V conversion" is the system spec. Is there anything we can do to solve this problem ? Also , changing to another buck IC is the last option.
Any suggestion is welcome. Thanks!