Hi,
I am FAE, a distributor of TI products.
My customer plans to create a circuit with the following specifications using the device of LMR36015A.
Currently, Fordback resistors are selected, but the following values are considered.
The resistance value is set lower than the data sheet selection requirements.
The reason is to reduce the influence of noise.
Is it possible to use the following values?
When VIN = 24V, VOUT = 1.2V
RFBB = 100kΩ, RFBT = 20kΩ
My customer plans to create a circuit with the following specifications using the device of LMR36015A.
Currently, Fordback resistors are selected, but the following values are considered.
The resistance value is set lower than the data sheet selection requirements.
The reason is to reduce the influence of noise.
Is it possible to use the following values?
When VIN = 24V, VOUT = 1.2V
RFBB = 100kΩ, RFBT = 20kΩ
When VIN = 24V, VOUT = 3.3V
RFBB = 27kΩ, BFBT = 62kΩ
RFBB = 27kΩ, BFBT = 62kΩ
Best regards,