Part Number: BQ25120A
Other Parts Discussed in Thread: BQ25121A, BQ25122, BQ25125
What are the differences in the BQ2512X family of devices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
| Device | VSYS | LS/LDO (Default) | VIN_DPM | Watchdog Timer | Other Features |
| BQ25120A | 1.8V | Load Switch | Enabled | Enabled | |
| BQ25121A | 2.5V | Load Switch | Enabled | Disabled | |
| BQ25122 | 1.2V | Load Switch | Enabled | Enabled | |
| BQ25125 | 1.8V | LDO (1.8V) | Disabled | Enabled | DPPM Disabled |
Please refer to the datasheet for more information.
LDO can be configured to either load switch or LDO mode though I2C.