This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 68
Part Number: TPS7A83A
Hi,
TPS7A83A works as a ANY-OUT operation. and currently, the SNS pin in connected directly to the output pin 1 on both schematic and layout. but the real remote load voltage is low than expected for path loss. so is it possible connect SNS pin to the remote load directly for more accuracy feed back to error amplifier? in this case, can output be improved a little bit when connect SNS to the remote load point?
Thank you very much.
Hi Liyu,
Yes, when using in any-out operation, SNS should be connected directly to the load side to improve the accuracy during heavy load.
Regards,
Jason Song
Please click the "Resolved" link at the bottom of this post if I have answered your question.