Other Parts Discussed in Thread: BQ25890
I want to discuss a few questions:
1: Regarding the charging process of the BQ24296m, where is point the CC mode entering the CV mode?
2: Is it looking at the battery voltage or capacity, or the charging current?
3: Can this point be adjusted?
4: When use 1S2P battery ,It's need to note what the design point of the BQ24296m?
I now see a phenomenon that I don't know if it is a problem.
We are use 1S2P 18650 battery. The capacity is increased more then one cell battery. I found that he was space very long time near full charger(1.5H~2H) more then one cell battery..
Our VREG is set to 4.208V, and the ITERM is set to 128mA. The battery is 18650 CELL, 1S2P, and the capacity is 6700mAh.