I have been reading out the default (on power up) values for the FC1 and FC2 registers and while most of the fields match what is documented in SLVA744.PDF, there are two fields in FC1 that don't. These fields are LODVTH and LOD_Removal_EN (as defined in Table 4). I am reading 0 for both of these fields. Is this normal, or do I have an issue to be concerned about?
** Tom **