Can anyone help or suggest a test regime please?
The attached PDF shows the power supply circuit of my project . The design is taken from the component data sheets with values calculated against the coil inductance Ls = 12u3H (quoted) and Ls' = 16u5H (extrapolated from other data).
I would anticipate a steady output at [OUT] when the coil is on the charger, regardless of load. I have tested with both a 'Chinese' wireless charger and a Samsung phone charger. The results are the same.
With a LiPo (open voltage 3v73) connected at [V_BATT], or no battery connected, I see LED_3 (!CHG_1) and LED_1 (!CHG) flash on momentarily, then after a short delay, repeat.
If I connect a faulty LiPo (open voltage 2v93), I see the same as above, but in addition LED_2 (!PG) comes on momentarily after LED_1
Lipo capacity 600mAh (quoted)