Other Parts Discussed in Thread: TIDA-00688, BQ51003,
Dear TI Experts,
we are developing a low power Qi receiver application according to the TIDA-00688 application note. Now we are facing problems with the little BGA pitch of BQ51003. The application is to price sensitive to switch to 4 layer and micro vias that are required to connect the inner BGA balls.
I would like to know if there are any restrictions to change the recommended BQ51003 with the BQ51013B. BQ51013B comes in a bigger package. I' m afraid that the maximum current of 240 mA and a usual current < 100 mA could be too low to keep the Qi power transfer alive?
Thanks,
Kilian