This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 69
Part Number: CSD95375Q4M
Hi Team,
may i have your help to know CSD95375Q4M Junction-to-ambient Thermal Resistance Theta-ja?
Henry,
Thanks for posting.
RthJA of a device is a function of both packageand thermal environment which is why whenever you see it specified on a datasheet, it is specified for a given board thickness and size.
A 5x6 QFN will have a RthJA of ~40deg C / W typically on a 1x1" 2oz Cu board. A 3x3 QFN will be closer to 50deg C / W on the same board. So this 3.5 x 4.5 would be somewhere in between, around 45deg C / W on a 1x1" 2oz Cu board. With thicker PCB, or other means of pulling heat out from the package, be it airflow or a heatsink, you might be able to get that down to 20deg C/W or less but again, that would depend on the design.
Best Regards!
Brett Barr
Product Marketing Engineer