Other Parts Discussed in Thread: LM3881
Hi Team,
My customer is planning on using our LM3881 to power the enable pin of the TPS22954. A concern of my customer is that the TPS22954 may turn on due to the Vflag votlage ramping up as it's input voltage ramps as well as seen in the table belwo for the LM3881.
The Vflag will be connected to the EN pin of the TPS22954 which has the below threshold voltage with min of 0.65V which is close to the VFLAG voltage spike.
I was hoping to check if the TPS22954 would be able to withstand that voltage without turning on prematurely?
Thanks!
BR,
Alfred